Edit a device type
If you want an edited version of a locked device type, you must create a new device type from it. Certain “standard” device types can be used to create new types, but they cannot be deleted. Examples: Circuit Monitor 4000, Power Meter 800, and Sepam S42.
NOTE: You cannot edit any locked device type. When a device type is locked, the locked icon displays on the Define Device Type Tags tab:
To edit a device type:
- Open Add / Edit Device Type: In Profile Editor, click Define Device Type Tags, then click Add / Edit (to the right of the Device Type Name field.)
There are two ways to edit device types:
- In Define Device Type Tags, select a device type and then make the following changes:
- Edit the functional address (see Edit functional addresses).
- In Real Time Tags you can edit the address (see Editing tag addresses) and choose a different format.
- In Define Device Type Tags, select the device type you want to edit, then click Add / Edit. Follow through the screens to edit additional information:
- In the Device Type Options box, click Edit Existing.
- Click the Device Type to Edit list to display the Select Device box. Select the device type that you want to edit.
- You can change the device type name, category, subcategory, and driver.
- Select tags and tag groups and move them into or out of the Selected Tags list.
- If a device type is associated with a device profile, you cannot deselect tags.
- After all of the appropriate changes are made, click Save to save your current settings.
- To create additional custom tags, click Add / Edit Custom Tags; otherwise, click Save & Exit to save your settings and close the window.
If you add a tag to a group that is already included in a device type, you must then individually add the tag to that device type.